Tag Browser and Data Type Browser customization methods
Tag Browser
and Data Type Browser
customization methodsUse the following methods to customize the appearance of the and the . Changes are saved for the logged on user.
Tag Browser
Data Type Browser
To do this: | Do this: |
Resize the browser. | Position the pointer on an edge of the browser window until the resizing arrow appears and then drag. |
Move the browser. | Position the pointer near an edge of the browser until the move arrow appears, and then drag. The move is temporary. When re-opened, the browser appears in the original location. |
Rearrange the columns. | Select the column heading and drag. The Name column is fixed and cannot be moved to another position. |
Resize a column. | Position the pointer over the column header row until the resizing arrow appears, and then drag. |
Show or hide a column. | Right-click a column heading and select or clear the column in the list to show or hide the column. |
Provide Feedback