What is binding?
Binding is the process of specifying the value of a property dynamically. Graphic element properties that are bound to data update automatically when the value of the data changes.
Bind a property of a graphic element or instance of an Add-On Graphic to a data item:
- A tag, including system tags. Browse for tags to bind to after you configure a controller reference on theProject Propertiesdialog box.
- Extended properties of tags.
- An expression. For example, to bind the property to the value of the expression, you can enter ::controller\program.tag1+::controller\program.tag2.
- A property of a graphic element or screen. For example, you can bind the Text property of TextDisplay_003 to TextDisplay_001.Text.
- Each referenced analog tag has eu/min/max.
- Each BOOLEAN tag references has state identifiers
- All tags have descriptions
From within the definition of an Add-On Graphic, you can only bind to an external data type property or the property of another graphic element within the definition of an Add-On Graphic.
Properties that you can bind display a
when you point to them.
Binding
button
when you point to them.
IMPORTANT:
- The HMI device updates data from controllers at a fixed rate of 100, 250, or 500 milliseconds. This update is asynchronous to any scan in a controller.
Provide Feedback