Example: Relational operators in expressions

These are the examples of relational operators in expressions.
Symbol (Function)
Description
Example: If tag1 = 5 and tag2 = 7, then:
== (Equal to)
Compares the two values and returns a 1 (true) if they are equal. Returns a 0 (false) if they are not equal. Performs a case-sensitive string comparison.
All values are converted to double-precision floating point first, and then the operation is performed.
tag1 == tag2
is false, so the expression returns 0
!= (Not equal to)
Compares the two values and returns a 1 (true) if they are not equal. Returns a 0 (false) if they are equal.
All values are converted to double-precision floating point first, and then the operation is performed.
tag1 != tag2
is true, so the expression returns 1
< (Less than)
Compares two values and returns a 1 (true) if the value on the left is smaller than the value on the right. Returns a 0 (false) if not.
All values are converted to double-precision floating point first, and then the operation is performed.
tag1 < tag2
is true, so the expression returns 1
> (Greater than)
Compares two values and returns a 1 (true) if the value on the left is larger than the value on the right. Returns a 0 (false) if not.
All values are converted to double-precision floating point first, and then the operation is performed.
tag1 > tag2
is false, so the expression returns 0
<= (Less than or equal to)
Compares two values and returns a 1 (true) if the value on the left is smaller or the same as the value on the right. Returns a 0 (false) if not.
All values are converted to double-precision floating point first, and then the operation is performed.
tag1 <= tag2
is true, so the expression returns 1
>= (Greater than or equal to)
Compares two values and returns a 1 (true) if the value on the left is larger or the same as the value on the right. Returns a 0 (false) if not.
All values are converted to double-precision floating point first, and then the operation is performed.
tag1 >= tag2
is false, so the expression returns 0
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal