Example: Punctuators in expressions

These are the examples of punctuators in expressions.
Symbol
Description
Example
( )
Opening and closing parentheses. Use parentheses around any subexpression to specify the order of operations. Subexpressions inside parentheses are evaluated prior to any operators outside the parentheses being applied.
3 + 2 * 6
returns
15
(3 + 2) * 6
returns
30
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal