Expression Editor
How do I open the Expression Editor?
From any input box where you can apply an expression, click
.
Open Expression Editor
Use the
Expression Editor
to create or edit lengthy or complex expressions in a resizable window. Most expressions consist of one or more tag references combined with numbers, mathematical operators, or built-in functions. However, a tag is not required in an expression.
View Designer
checks the expression syntax as you create the expression. A redView Designer
also verifies the syntax for all expressions in a project before it is downloaded to the HMI device. In addition, it verifies that tag references exist in the controller projects. It also verifies that the property of a graphic element referenced in an expression exists in the screen where it exists. If there are invalid expressions, the download process stops, and the invalid expressions appear in the Errors
window. Verify expressions any time during the project development process by using the PROJECT > Verify Project
command.Provide Feedback