Change an expression
Change an expression, for example, to select a different tag. Changes to an expression save automatically.
To change an expression
- Type the changes directly into the expression/binding box.
- Open theExpression Editorand make changes to the expression in the editor.TIP:To change a tag in an expression from within the definition of an Add-On Graphic, click the tag link in the expression to open theTag Browser. The tag in the expression is selected in theTag Browserautomatically. Select a different tag to change the expression.
Provide Feedback