Property-to-property binding
Property-to-property binding binds the property of one graphic element to the same property of another graphic element on the screen. If the graphic elements display a value in different formats, the graphic elements show the same value on the HMI device. This example depicts binding the value property of a numeric display to the Level property of a mixer to show the level graphically and numerically on the HMI device.

Graphic elements on a screenItem | Description |
![]() | A MixingHopperSide_001 graphic element on a screen. The value of the MixingHopperSide_001 graphic element is bound to the Level tag. Browse to the controller tag to show the value on the HMI device. The value of the Level shows graphically on the mixing hopper on the HMI device. |
![]() | A NumericDisplay_001 graphic element on the same screen. The value of the NumericDisplay_001 graphic element is bound to the Level property of the mixing hopper graphic element. To bind the property of one graphic element to the property of another graphic element, use the format ElementName.PropertyName. The value of Level shows numerically on the numeric display on the HMI device. |
Graphic elements on the HMI deviceItem | Description |
![]() | The mixing hopper graphic element and the numeric display graphic element show the level of the mixer on the HMI device. |
Provide Feedback