What can be used as an Expression Value in a Color Table or State Table
Specify a single value or a value range for an Expression Value in a
Color Table
or in a State Table
. An Expression Value can be:- An integer number.Any positive or negative number up to 15 digits.
- A floating point number.Any positive or negative number up to 15 significant digits in the range of ±1.7 x 10±308.
- A string.Any sequence of alpha-numeric characters enclosed in quotation marks.
Provide Feedback