Change an animation

After creating an animation for a graphic element, including an Add-On Graphic, or screen, modify it. For example, adjust the value that drives the animation.
TIP:
If an event references a
State Table
and then the name of the table changes, change the reference to reflect the new
State Table
name.
View Designer
does not automatically update references with the new name.
To change an animation
  1. Select the graphic element, Add-On Graphic, or screen that contains the animation to change.
  2. On the
    Properties
    window, select the
    Animations
    tab.
  3. Select the appropriate
    State Table
    or
    Color Table
    .
  4. Change any or all of the properties in the table. Changes are saved automatically.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal