Change the PDF document that appears on an HMI device

Change the PDF document referenced on a screen, popup, or Add-On Graphic to view a different PDF document on the HMI device.
To change the PDF document that appears on an HMI device
  1. On the screen, select the PDF graphic element or PDF_Viewer Add-On Graphic that references the PDF document.
  2. In the
    Properties
    window, select the
    Properties
    tab and expand the
    General
    category.
  3. In the
    DocumentName
    box, select a different PDF document.
    TIP:
    A
    No document assigned
    message appears when the PDF graphic element or a PDF Viewer Add-On Graphic does not reference a PDF document.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal