Add a PDF graphic element to a screen, popup, or Add-On Graphic
Add a PDF graphic element to a screen, popup, or Add-On-Graphic from the
Toolbox
to display the PDF document on the HMI device. PDF graphic elements exist in the Toolbox
. The PDF document that a PDF graphic element references exists in the Documents
folder of the Project Explorer
.Prerequisites
- (optional) Create bookmarks for the PDF document prior to adding the document to the project.
To add a PDF graphic element to a screen or popup, or Add-On Graphic
- From theToolbox, expand theSystemcategory and then double-click or drag the PDF graphic element to a screen, popup, or definition of an Add-On Graphic.
- On theSelect Documentdialog box, either:
- Select an existing PDF document and selectOK.
- SelectBrowse, select a new PDF document or multiple PDF documents, selectOpento add the documents to theSelect Imagedialog box, select the PDF document to add to the screen, and then selectOK.The PDF graphic element appears on the screen and references the PDF document.TIP:Tips:
- Browsing to and selecting multiple PDF documents in theSelect Documentdialog box highlights the last selected PDF document.
- SelectingCancelon theSelect Documentdialog box places a PDF graphic element on the screen. The PDF graphic element displays a message to add a PDF document to the PDF graphic element.
- In thePropertieswindow, select thePropertiestab. The properties for that item appear in categories.
- Expand a category to display a property and change the value or bind a property.TIP:Tips:
- To add a PDF Viewer Add-On Graphic configured with touch navigation and zoom commands, add a PDF Viewer Add-On Graphic from theAdd-On Graphicscategory of theToolbox.
- Adding a PDF document from theAssets > Documentsfolder of theProject Exploreropens theSelect PDF Viewerdialog box to select the PDF Viewer Add-On Graphic or PDF graphic element to display the PDF document on the HMI device.
- PDF documents on the HMI device support internal links for navigation within the PDF document. PDF documents on the HMI device do not support external links. PDF links cannot navigate outside of the PDF document on the HMI device.
- PDF files that contain complex drawings take longer to render. For example, if a PDF document contains an image comprised of individual shapes such as lines, circles, and rectangles, that image takes longer to render than a drawing that is a single image.
- Do not rotate the PDF graphic element or a PDF Viewer Add-On Graphic. Rotating an element containing a PDF document reduces the clarity of content in the PDF document and prevents zooming and navigating the PDF document on the HMI device.
Provide Feedback