Select Image dialog box

How do I open the Select Image dialog box?
In
Toolbox > CommonControls
, double-click the Image graphic element.
Use the
Select Image
dialog box to reference a new or existing image that the Image graphic element displays on the screen.
The
Select Image
dialog box lists the existing images in the
Images
folder of the
Project Explorer
and and enables browsing to new images. Selected images appear in the
Images
folder.
The
Images
folder is in the
Assets
folder of the
Project Explorer
.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal