Replace an image throughout a project

Replace an image in the
Images
folder to replace the image wherever it is referenced in the project.
To replace an image in the Images folder:
  1. In the
    Project Explorer
    , right-click the
    Images
    folder and select
    New Images.
  2. Browse to and select the replacement image. The replacement image must have the same file name as the existing image.
  3. Select
    Yes
    . The image is replaced and all instances of the referenced image are replaced with the latest version.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal