Replace an image on a screen
Replacing an image on a screen references the new image in the Image graphic element. Link an image to an Image graphic element that has no referenced image. An Image graphic element shows a red X when it has no referenced image. Change the image referenced by an Image graphic element.
To replace an image on a screen
- Select the Image graphic element on the screen.
- In thePropertieswindow, select thePropertiestab and expand theGeneralcategory.
- Select the down arrow in theImageNamebox. A list of the images in theImagesfolder appears.
- Select an image name. The image scales to fit the Image graphic element but does not maintain its aspect ratio.
Provide Feedback