Preview an image
Open a read-only version of the image to preview the image before adding it to a screen. Preview images exist in the
Assets > Images
folder of the project. To preview an image
- In theProject Explorer, expand theAssets > Imagesfolder.
- Double-click the image. A tab opens with a read-only version of the image.TIP:Tips:
- The property values for the file name, type, size, and the memory the image requires on the HMI device are read-only.
- Right-clicking an image in theAssets > Imagesfolder and selectingOpenpreviews an image.
Provide Feedback