Image naming conventions

Image names have the following considerations:
  • Invalid characters in file names are removed from the file name.
  • Characters after the 40-character limit in a file name are removed.
  • Underscores replace spaces in the file name.
  • Files created with the same name as a system-defined file name have file names that increment with an underscore and a number from 001 to 999.
    For example, adding an image file named 01_picture.png adds an image named picture.png to the the
    Images
    folder. Adding an image file named 02_picture.png adds an image named picture_001.png to the
    Images
    folder.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal