Delete an image from a project
Deleting an image from a project:
- Removes the image from all screens in the project that use the image.
- Deletes the references to the image wherever it is used in the project.
- Clears the ImageName property in thePropertiestab for each Image graphic element that references the ImageName.
The Image graphic element displays a red X on the screen when it has no referenced image.
IMPORTANT:
Deleting an image deletes the references to the image. Adding the image back to the
Images
folder does not restore the configuration. To delete an image from a project
- In theProject Explorer, open theAssets > Imagesfolder.
- Right-click the image and clickDelete. A prompt appears if an Image graphic element in the project uses the image.
- ClickYesto delete the image file. ClickNoto and keep the file.
Provide Feedback