Zoom in or zoom out
Zoom in on a screen, shortcut, popup, the to enlarge it and all of its contents. For example, zoom in to edit a small, complex portion of a screen. Zoom out to reduce the size of the contents. For example, zoom out to view an entire screen to preview how it appears on the HMI device.
System Banner
, or the definition of an Add-On GraphicTo zoom in or zoom out:
- On theScreen Editor toolbar, or select
to zoom in or select
to zoom out. The minimum zoom is 10%. The maximum zoom is 500%. The toolbar displays the current zoom level.TIP:Tips:- To use the keyboard and mouse to zoom in or out, press theCtrlkey and rotate the wheel of the mouse.
- To view the entire screen, shortcut, popup,System Banner, or Add-On Graphic definition, selectFit to Window
. - To reset the screen, shortcut, popup,System Banner, or Add-On Graphic definition to actual size, pressCtrl+1.
- The zoom level is not maintained when closing the screen or project.
Provide Feedback