Select a graphic element in the Graphic Explorer
Select one or more graphic elements in the
Graphic Explorer
to perform actions on them or display their properties. To select a graphic element in the Graphic Explorer:
- SelectView > Graphic Explorerto open theGraphic Explorer.
- (optional) If the graphic element is contained in a group, expand the group in theGraphic Explorer.
- To select:
- A single graphic element, select the graphic element.
- Multiple graphic elements, press and holdCtrlwhile you select each element.TIP:To deselect the selected graphic elements, select the screen.
Provide Feedback