Flip a graphic element

Flip a graphic element or Add-On Graphic to create a reverse image of the element.
To flip a graphic element:
  1. On the screen or in the
    Graphic Explorer
    , right-click the graphic element and select
    Flip
    .
  2. Select one of the following options:
    • Horizontal
      . Flips the graphic element along its horizontal axis.
    • Vertical
      . Flips the graphic element along its vertical axis.
      TIP:
      Tips:
      • Alternate methods to flip a graphic element:
        • On the
          Drawing
          toolbar, select the
          Flip
          down arrow, and select an option.
        • Select
          Arrange > Flip
          , and select an option.
      • Flipping a graphic element that contains text does not flip the text.
      • Flip rotated graphic elements. The new rotation angle displays in the Angle property for the graphic element.
      • Flipping groups of graphic elements is supported. Flipping individual graphic elements within a group is not supported.
      • When flipping a graphic element in the definition of an Add-On Graphic, the background of the Add-On Graphic may resize to fit the flipped graphic element.
      • Flipping screens, popups, the definition of an Add-On Graphic, or the
        System Banner
        is not supported.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal