Duplicate a graphic element
Use the
Duplicate
command to make a copy of a graphic element or Add-On Graphic. When duplicating a graphic element, everything associated with the graphic element, including property values, animations, and events, is also duplicated.To duplicate a graphic element:
- On the screen or in theGraphic Explorer, select the graphic element or group of graphic elements and pressCtrl+D.TIP:Tips:
- Duplicating a graphic element within the definition of an Add-On Graphic is supported.
- Create copies until de-selecting the graphic element or group.
- The duplicate function does not use the clipboard. The contents of the clipboard are not affected when duplicating graphic elements.
Provide Feedback