Distribute graphic elements

Distribute graphic elements and Add-On Graphics to space them evenly and horizontally or vertically on the screen.
View Designer Distributing Horizontal after
View Designer Distributing Horizontal after
View Designer Distributing Horizontal after
To distribute graphic elements:
  1. On the screen, select at least three graphic elements to distribute. The outermost graphic elements act as end points for distribution.
  2. Right-click one of the selected graphic elements and select
    Distribute
    .
  3. Select
    Horizontal
    or
    Vertical
    .
    TIP:
    The background of an Add-On Graphic may resize when distributing graphic elements in the definition of the Add-On Graphic.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal