Delete a graphic element
Delete a graphic element or Add-On Graphic from a screen or from the
Graphic Explorer
. Deleting a graphic element or Add-On Graphic from a screen or the Graphic Explorer
does not delete it from the Toolbox
. To delete a graphic element:
- On the screen or in theGraphic Explorer, select the graphic element or Add-On Graphic and pressDelete.TIP:Tips:
- To delete an Add-On Graphic from a project, delete all instances of the Add-On Graphic from the project and then delete the Add-On Graphic from theProject Explorer.
- Alternate methods of deleting a graphic element include:
- Right-clicking the element and selectingDelete.
- Selecting the element and pressingCtrl+X.
- To select multiple graphic elements to delete, holdCtrlwhile selecting each graphic element.
Provide Feedback