Draw an oval or circle
Use the
Ellipse Tool
to draw an oval or a circle.To draw an oval or circle:
- In theToolbox, select theEllipse Tool
. - On the screen, select where the oval or circle is to begin.
- To draw anoval, drag to the desired size.
- To draw acircle, press and holdShiftand drag.TIP:Tips:
- Use Smart Guides to help position the shape.
- To change the shape of an oval or circle, use the sizing handles.
- The selected drawing tool remains active until selecting a different drawing tool.
Provide Feedback