Draw an arc
Use the
Arc Tool
to draw a curved line on the screen.To draw an arc
- In theToolbox, select theArc Tool
. - On the screen, select the beginning point of the arc.
- Select a second point to determine the span and the direction of the arc.
- Select a third point to determine the height of the arc.TIP:Tips:
- Use Smart Guides to position the shape.
- The selected drawing tool remains active until you select a different drawing tool.
Provide Feedback