Draw a rectangle or square
Use the
Rectangle Tool
to draw rectangles or squares. To draw a rectangle or square:
- In theToolbox, select theRectangleTool
. - On the screen, position the crosshair where the square or rectangle is to begin.
- To draw arectangle, click and drag.
- To draw asquare, press and holdShiftand drag.TIP:Use Smart Guides to help position the shape.
Provide Feedback