Draw a line, polyline, or polygon
Use the
Line Tool
to draw a line, or the Pen Tool
to draw a polyline, polygon, or line.To draw a line, polyline, or polygon:
- In theToolbox, select a tool to draw the item:
- Line.Select theLine Tool
and drag to draw the line. - Polyline.Select thePenTool
and select points on thescreen. - Polygon.Select thePenTool
, select points on the screen, and then select the initial point to close the polyline shape. TIP:Tips:- Selecting thePenTool
and selecting a start and end point draws a line. - Use Smart Guides to help position the line.
- To change the shape of a polyline or polygon, select the sizing handle in the middle of a line segment.
- To remove a segment from a polyline or polygon, select the sizing handle at the end of the segment.
- The selected drawing tool remains active until selecting a different drawing tool.
Provide Feedback