FluidPower
The
FluidPower
category under SignsAndSymbosl
in the Toolbox
contains valves and pneumatic symbols. These graphic elements are commonly used to depict a fluid power system. Add values and the pneumatic symbols to depict a power system that uses water.
Unique properties
Unique properties are properties that not all graphic elements in the
Toolbox
share.Name | Category | Purpose | Accepted values |
BorderColor | Appearance | Specifies the border color. | Any selected color in the Color Picker or a Hex color value entered manually. The Hex value must be in the format #RRGGBB. R, G, and B are Hex digits from 0 through F and represent the color channel values for red, green, and blue. For example, #ffff00 produces yellow. |
FillColor | Appearance | Specifies the fill color. | Any selected color in the Color Picker or a Hex color value entered manually. The Hex value must be in the format #RRGGBB. R, G, and B are Hex digits from 0 through F and represent the color channel values for red, green, and blue. For example, #ffff00 produces yellow. |
Common properties exist for all graphic elements.
Property | Category | Purpose | Accepted Values |
Access | Security | Specifies if all users have access to the control element, or if access is inherited from the screen. |
|
Angle | Position and Size | Specifies the rotation angle. Enter 180 to display the graphic element upside down. If you enter a value larger than 360, the portion of numeric value that is over 360 becomes the value. For example, enter 380 to see a value of 20. If you enter a value less than 0, the negative value is subtracted from 360. For example, enter -30 to see a value of 330. |
|
Enabled | Appearance | Specifies if the graphic element is available on the HMI device and if the graphic element accepts touch and key input. |
|
Height | Position and Size | Specifies the height in pixels. | Any positive numeric value |
Opacity | Appearance | Specifies the transparency of the graphic element. | 0 (fully transparent) - 100 (fully opaque) |
Visible | Appearance | Specifies if the graphic element is visible on the HMI device. |
|
Width | Position and Size | Specifies the width in pixels. | Any positive number |
X | Position and Size | Specifies the horizontal coordinate, in pixels, from the upper left corner of screen to the upper left corner of a graphic element or group with no rotation. If the graphic element or group is rotated, the X property value does not change. | Any positive number |
Y | Position and Size | Specifies the vertical coordinate, in pixels, from the upper left corner of screen to the upper left corner of a graphic element or group with no rotation. If the graphic element or group is rotated, the Y property value does not change. | Any positive number |
Provide Feedback