Graph
The
Graphs
category under GeneralEquipment
in the Toolbox
contains graphic elements to display data on bar graphs and spider charts. These graphic elements are commonly used to display data in a manufacturing system.Add a bar graph that shows the amount filled or a spider chart that displays the status of three to seven tag values, depending on the spider chart selected. For example, to display the status of four tag values, add the Spider Chart 4 graphic element and bind the built-in animation properties of the graphic element to a tag. The values from a controller are plotted on the chart or graph when the values are read from the controller.
Built-in animation properties
Built-in animation properties appear under the
General
category of the Properties
window. Specify values for these properties in order to animate the graphic element or change the information the graphic element shows on the HMI device.Not all graphic elements in this category have the same properties. The built-in animation properties for a graphic element in this category depend on the graphic element selected. For example, the Input values for a Spider Chart 4 include Input1 through Input4, Input1Min through Input4Min, and Input1Max through Input4Max.
Name | Category | Purpose | Accepted values |
Input1 | General | Specifies the value for the first dimension in the spider chart. | Bound tag |
Input2 | General | Specifies the value for the second dimension in the spider chart. | Bound tag |
Input3 | General | Specifies the value for the third dimension in the spider chart. | Bound tag |
Input4 | General | Specifies the value for the fourth dimension in the spider chart. | Bound tag |
Input5 | General | Specify the value for the fifth dimension in the spider chart. | Bound tag |
Input6 | General | Specifies the value for the sixth dimension in the spider chart. | Bound tag |
Input7 | General | Specifies the value for the seventh dimension of the spider chart. | Bound tag |
Input1Max | General | Specifies the maximum value for the first dimension in the spider chart. | Any value greater than the Input1Min property value |
Input2Max | General | Specifies the maximum value for the second dimension in the spider chart. | Any value greater than the Input2Min property value |
Input3Max | General | Specifies the maximum value for the third dimension in the spider chart. | Any value greater than the Input3Min property value |
Input4Max | General | Specifies the maximum value for the fourth dimension in the spider chart. | Any value greater than the Input4Min property value |
Input5Max | General | Specifies the maximum value for the fifth dimension of the spider chart. | Any value greater than the Input5Min property value |
Input6Max | General | Specifies the maximum value for the sixth dimension of the spider chart. | Any value greater than the Input6Min property value |
Input7Max | General | Specifies the maximum value for the seventh dimension in the spider chart. | Any value greater than the Input7Min property value |
Input1Min | General | Specifies the minimum value for the first dimension in the spider chart. | Any value less than the Input1Max property value |
Input2Min | General | Specifies the minimum value for the second dimension in the spider chart. | Any value less than the Input2Max property value |
Input3Min | General | Specifies the minimum value for the third dimension in the spider chart. | Any value less than the Input3Max property value |
Input4Min | General | Specifies the minimum value for the fourth dimension in the spider chart. | Any value less than the Input4Max property value |
Input5Min | General | Specifies the minimum value for the fifth dimension of the spider chart. | Any value less than the Input5Max property value |
Input6Min | General | Specifies the minimum value for the sixth dimension in the spider chart. | Any value less than the Input6Max property value |
Input7Min | General | Specifies the minimum value for the seventh dimension of the spider chart. | Any value less than the Input7Max property value |
MaxValue | General | Specifies the maximum value on the graphic element. | Any numeric value greater than the MinValue property value |
MinValue | General | Specifies the minimum value on the graphic element. | Any numeric value less than the MaxValue property value |
Value | General | Specifies the value of the graphic element. | Bound tag |
Unique properties are properties that not all graphic elements in the Toolbox share. Not all graphic elements in this category have the same properties. The unique properties of a graphic element in this category depend on the graphic element selected.
Name | Category | Purpose | Accepted values |
Color | Appearance/Axis | Specifies the color of the lines on the spider chart. | Any selected color in the Color Picker or a Hex color value entered manually. The Hex value must be in the format #RRGGBB. R, G, and B are Hex digits from 0 through F and represent the color channel values for red, green, and blue. For example, #ffff00 produces yellow. |
Color | Appearance/Border | Specifies the color of the border. | Any selected color in the Color Picker or a Hex color value entered manually. The Hex value must be in the format #RRGGBB. R, G, and B are Hex digits from 0 through F and represent the color channel values for red, green, and blue. For example, #ffff00 produces yellow. |
CornerRadius | Appearance | Specifies the curve of the corners. | 0 or a positive number |
FillColor | Appearance | Specifies the fill color. | Any selected color in the Color Picker or a Hex color value entered manually. The Hex value must be in the format #RRGGBB. R, G, and B are Hex digits from 0 through F and represent the color channel values for red, green, and blue. For example, #ffff00 produces yellow. |
LevelColor | Appearance | Specifies the color of the fill level. | Any selected color in the Color Picker or a Hex color value entered manually. The Hex value must be in the format #RRGGBB. R, G, and B are Hex digits from 0 through F and represent the color channel values for red, green, and blue. For example, #ffff00 produces yellow. |
Style | Appearance/Axis | Specifies the style of the lines on the spider chart. |
|
Style | Appearance/Border | Specifies the style of the border line. |
|
Width | Appearance/Axis | Specifies the width of the lines on the spider chart. |
|
Width | Appearance/Border | Specifies the width of the border line. |
|
Common properties exist for all graphic elements.
Property | Category | Purpose | Accepted Values |
Access | Security | Specifies if all users have access to the control element, or if access is inherited from the screen. |
|
Angle | Position and Size | Specifies the rotation angle. Enter 180 to display the graphic element upside down. If you enter a value larger than 360, the portion of numeric value that is over 360 becomes the value. For example, enter 380 to see a value of 20. If you enter a value less than 0, the negative value is subtracted from 360. For example, enter -30 to see a value of 330. |
|
Enabled | Appearance | Specifies if the graphic element is available on the HMI device and if the graphic element accepts touch and key input. |
|
Height | Position and Size | Specifies the height in pixels. | Any positive numeric value |
Opacity | Appearance | Specifies the transparency of the graphic element. | 0 (fully transparent) - 100 (fully opaque) |
Visible | Appearance | Specifies if the graphic element is visible on the HMI device. |
|
Width | Position and Size | Specifies the width in pixels. | Any positive number |
X | Position and Size | Specifies the horizontal coordinate, in pixels, from the upper left corner of screen to the upper left corner of a graphic element or group with no rotation. If the graphic element or group is rotated, the X property value does not change. | Any positive number |
Y | Position and Size | Specifies the vertical coordinate, in pixels, from the upper left corner of screen to the upper left corner of a graphic element or group with no rotation. If the graphic element or group is rotated, the Y property value does not change. | Any positive number |
Provide Feedback