Slider Horizontal
Use the
Slider Horizontal
graphic element to build an application using slider control. The Slider Horizontal
graphic element appears in the CommonControls
category of the Toolbox
. Built-in-Animation Properties
Built-in animation properties appear under the
General
category of the Properties
window. Specify values for these properties in order to animate the graphic element or
change the information the graphic element shows on the HMI device.
NOTE:
The Value property of the slider is always treated as a floating
point value, even if the slider limits are set to 0 and 1 and the slider Value property is
bound to a BOOL tag.
Property | Category | Purpose | Accepted Values |
Value | General | Specifies the value of the graphic element | Bound tag |
MinValue | General | Specifies the minimum value on the graphic element | Any numeric value less than the MaxValue property value. |
MaxValue | General | Specifies the maximum value on the graphic element | Any numeric value greater than the MinValue property value. |
Write Mode | General | Specifies when the control updates the value tag | Continuous Update - Updates the tag bound to the value property while
dragging the slider thumb along the trackUpdate on Release - Updates the tag bound to the value property after
releasing the slider thumb. |
Unique Properties
Unique properties are not shared by all graphic elements in
Toolbox
.Name | Category | Purpose | Accepted Values |
|---|---|---|---|
CornerRadius | Appearance | Specifies the curve of button corners. | Zero or a positive number. |
UsePredefinedDisabled | Appearance | Specifies the crosshatch overlay on disabled graphic element. | True or false |
FillColor | Appearance | Specifies the fill color. | Any selected color in the Color Picker or a Hex color value entered manually. The Hex value must be in the format #RRGGBB. R, G, and B are Hex digits from 0 through F and represent the color channel values for red, green, and blue. For example, #ffff00 produces yellow. |
BorderColor | Appearance/Border | Specifies the border color of the graphic element. | Any selected color in the Color Picker or a Hex color value entered manually. The Hex value must be in the format #RRGGBB. R, G, and B are Hex digits from 0 through F and represent the color channel values for red, green, and blue. For example, #ffff00 produces yellow. |
BorderStyle | Appearance/Border | Specifies the border style for the graphic element. |
|
BorderWidth | Appearance/Border | Specifies the border width for the graphic element. |
|
ThumbStyle | Appearance/Thumb | Specifies the appearance of the slider thumb. |
|
ThumbFillColor | Thumb | Specifies the fill color for the slider thumb. | Any selected color in the Color Picker or a Hex color value entered manually. The Hex value must be in the format #RRGGBB. R, G, and B are Hex digits from 0 through F and represent the color channel values for red, green, and blue. For example, #ffff00 produces yellow. |
ThumbBorderColor | Thumb | Specifies the border color for the slider thumb. | Any selected color in the Color Picker or a Hex color value entered manually. The Hex value must be in the format #RRGGBB. R, G, and B are Hex digits from 0 through F and represent the color channel values for red, green, and blue. For example, #ffff00 produces yellow. |
ThumbThickness | Thumb | Adjusts the size of the thumb width along the track. | Zero or a positive number. |
TrackVisible | Track | Specifies visibility of the slider track element. | Enable or Disable |
TrackFillColor | Track | Specifies the fill color for the slider track. | Any selected color in the Color Picker or a Hex color value entered manually. The Hex value must be in the format #RRGGBB. R, G, and B are Hex digits from 0 through F and represent the color channel values for red, green, and blue. For example, #ffff00 produces yellow. |
TrackBorderColor | Track | Specific the border color for the slider track. | Any selected color in the Color Picker or a Hex color value entered manually. The Hex value must be in format #RRGGBB. R, G, and B are Hex digits from 0 through F and represent the color channel values for red, green, and blue. For example, #ffff00 produces yellow. |
TrackThickness | Track | Specifies the relative thickness of the slider track. | The percentage (0 to 100) of the height for Slider Horizontal or the percentage of the width for Slider Vertical. |
TrackCornerRadius | Track | Specifies the curve of the track. | Zero or a positive number |
LimitVisible | Track | Specifies the visibility of the range between the LowLimit and HighLimit . | Enable or Disable |
LowLimit | Track | Specifies the LowLimit value between the MinValue and MaxValue . | Any numeric value less than the HighLimit. |
HighLimit | Track | Specifies the HighLimit value between the MinValue and MaxValue . | Any numeric value greater than the LowLimit . |
LimitFillColor | Track | Specifies the fill color for the range between the LowLimit and HighLimit .Tip: Enable TrackVisible and LimitVisible before configuring LimitFillColor . The LimitFillColor property goes inactive after disabling TrackVisible and LimitVisible . | Any selected color in the Color Picker or a Hex color value entered manually. The Hex value must be in the format #RRGGBB. R, G, and B are Hex digits from 0 through F and represent the color channel values for red, green, and blue. For example, #ffff00 produces yellow. |
OutofLimitFillColor | Track | Specifies the fill color for the thumb and a portion of the track when the LowLimit and HighLimit are outside the MinValue and MaxValue range.Tip: Enable TrackVisible and LimitVisible before configuring LimitFillColor . The OutofLimitFillColor property goes inactive after disabling TrackVisible and LimitVisible . | Any selected color in the Color Picker or a Hex color value entered manually. The Hex value must be in the format #RRGGBB. R, G, and B are Hex digits from 0 through F and represent the color channel values for red, green, and blue. For example, #ffff00 produces yellow. |
Common Properties
Common properties exist for all graphic elements.
Property | Category | Purpose | Accepted Values |
Access | Security | Specifies if all users have access to the control element, or if access is inherited from the screen. |
|
Angle | Position and Size | Specifies the rotation angle. Enter 180 to display the graphic element upside down. If you enter a value larger than 360, the portion of numeric value that is over 360 becomes the value. For example, enter 380 to see a value of 20. If you enter a value less than 0, the negative value is subtracted from 360. For example, enter -30 to see a value of 330. |
|
Enabled | Appearance | Specifies if the graphic element is available on the HMI device and if the graphic element accepts touch and key input. |
|
Height | Position and Size | Specifies the height in pixels. | Any positive numeric value |
Opacity | Appearance | Specifies the transparency of the graphic element. | 0 (fully transparent) - 100 (fully opaque) |
Visible | Appearance | Specifies if the graphic element is visible on the HMI device. |
|
Width | Position and Size | Specifies the width in pixels. | Any positive number |
X | Position and Size | Specifies the horizontal coordinate, in pixels, from the upper left corner of screen to the upper left corner of a graphic element or group with no rotation. If the graphic element or group is rotated, the X property value does not change. | Any positive number |
Y | Position and Size | Specifies the vertical coordinate, in pixels, from the upper left corner of screen to the upper left corner of a graphic element or group with no rotation. If the graphic element or group is rotated, the Y property value does not change. | Any positive number |
Provide Feedback