Numeric Input
The Numeric Input graphic element is a control with built-in animation properties to show a tag value and open the virtual numeric keypad to change the value. Numeric Input appears under
Common Controls
in the Toolbox
.Use the Numeric Input graphic element to show the operator numeric information from the data source and to enable the operator to write a numeric value to the data source using the
Virtual Numeric Keypad
or inline editing.By default, the
Virtual Numeric Keypad
opens on PanelView
projects when interacting with a Numeric Input graphic element.The range of input values that can be entered in the virtual numeric keypad are specified by the
KeypadMaxValue
and KeypadMinValue
property values.Mask the value displayed in the graphic element and in the virtual numeric keypad by selecting the
MaskedValue
box in the Properties
window.Bind the
Value
property to a numeric tag (DINT, INT, SINT, or REAL). Bind the Value
property to a string tag if the string consists of only numerals. For example, the string value 456 displays as an integer and the string value 321.0 displays as a floating-point value.Use the
Rounding
field to specify how the numeric tag value appears when the amount of decimal places used by the numeric tag value exceeds the DigitsAfterDecimal
value. For example, if DigitsBeforeDecimal
is 3, DigitsAfterDecimal is 2, and Rounding
= Nearest, the value 112.345 displays as 112.35.
TIP:
Tips:
- If theValueproperty is assigned to an integer tag, theDigitsAfterDecimalproperty value is ignored. For example, ifDigitsBeforeDecimalis 3 andDigitsAfterDecimalis 1, the INT tag value 123 displays as 123 instead of 123.0.
- If theValueproperty is unassigned, the numeric display fills with asterisks.
- If the value does not fit within the bounding box of the graphic element, the numeric display is filled with asterisks.
- If the integer portion of the value, including the minus sign, contains more digits than specified for the display, the numeric display shows the value in scientific notation.
- If the number of characters required to show the value in scientific notation exceeds the sum of theDigitsBeforeDecimalandDigitsAfterDecimalfields, the numeric display fills with asterisks.
- If the value contains invalid characters, the numeric display shows dashes in place of the value. An error message appears above the graphic element.
- To change the method for entering values in this graphic element, change the ValueEntryMethod property for the graphic element. The ValueEntryMethod property specifies whether entering values is inherited from the project properties, performed through theVirtual Numeric Keypad.
Built-in animation properties appear under the
General
category of the Properties
window. Specify values for these properties in order to animate the graphic element or change the information the graphic element shows on the HMI device. Property | Category | Purpose | Accepted Values |
Value | General | Specifies the value of the graphic element. | Bound tag |
Unique properties are properties that not all graphic elements in the
Toolbox
share.Property | Category | Purpose | Accepted Values |
- CornerRadiusAppearanceSpecifies the curve of the corners.0 or a positive numberFillColorAppearanceSpecifies the fill color.Any selected color in theColor Pickeror a Hex color value entered manually. The Hex value must be in the format #RRGGBB. R, G, and B are Hex digits from 0 through F and represent the color channel values for red, green, and blue. For example, #ffff00 produces yellow.TextAlignmentAppearanceSpecifies the vertical and horizontal alignment of the text.Vertical alignment:
- Top
- Center
- Bottom
Horizontal alignment:- Left justified
- Centered
- Right justified
ColorAppearance/BorderSpecifies the color of the border.Any selected color in theColor Pickeror a Hex color value entered manually. The Hex value must be in the format #RRGGBB. R, G, and B are Hex digits from 0 through F and represent the color channel values for red, green, and blue. For example, #ffff00 produces yellow.StyleAppearance/BorderSpecifies the style of the border line.- Any selected Line style - None, Solid, Dash, Dot, Dash Dot, or Dash Dot Dot
- Any selected Cap style - Flat, Round, or Square
- Any selected Join style - Miter, Bevel, or Round
WidthAppearance/BorderSpecifies the width of the border line.- None
- 1 point
- 2 point
- 4 point
- 8 point
FontNameAppearanceSpecifies the font of the text.Any selected fontFontColorAppearanceSpecifies the color of the text.Any selected color in theColor Pickeror a Hex color value entered manually. The Hex value must be in the format #RRGGBB. R, G, and B are Hex digits from 0 through F and represent the color channel values for red, green, and blue. For example, #ffff00 produces yellow.FontSizeAppearanceSpecifies the size of the text.Positive numbersBoldAppearanceMakes the text or value on the graphic element bold.- Bold - selected
- Not bold - cleared
PaddingAppearanceSpecifies the distance, in points, between the content of the element and the edge of the element.Any numeric valueUsePredefinedDisabledAppearanceSpecifies if a crosshatch overlay shows on the control element when you disable the element.- Use predefined disabled appearance(selected)
- Do not use predefined disabled appearance(cleared)
DigitsBeforeDecimalNumericSpecifies the number of digits before the decimal point.0 - 9DigitsAfterDecimalNumericSpecifies the number of digits after the decimal point.0 - 9LeadingZeroNumericPlaces a zero before REAL numbers that are less than 1.- Leading zero (selected)
- No leading zero (cleared)
TrailingZerosNumericSpecifies that zeros fill the remaining decimal places.- Trailing zeros (selected)
- No trailing zeros (cleared)
RoundingNumericSpecifies the rounding method for the decimal portion of REAL numbers.- None - Do not round the number
- Up - Round up to the nearest number
- Nearest - Round up or down to the nearest number
MaskedValueInputSpecifies that asterisks mask the value entered on the numeric keypad.- Value masked (selected)
- Value not masked (cleared)
KeypadMaxValueInputSpecifies the maximum value to show and enter on the numeric keypad.Any numeric value that is greater than the KeypadMinValue property valueKeypadMinValueInputSpecifies the minimum value to show and enter on the numeric keypadAny numeric value that is less than the KeypadMaxValue property valueValueEntryMethodInputSpecifies the method for entering values in the graphic element. The default is to inherit the value entry method from the project. Selecting the virtual keypad value entry method overrides the default setting of the project.- InheritProjectSetting
- VirtualKeypad
When binding to this property, use either the name of a value or the associated number:- 0 (InheritProjectSetting)
- 1 (VirtualKeypad)
KeypadPositionInputSpecifies the position of the virtual numeric keypad on the screen. The default position is the center of the screen (Middle-center).- Top-left
- Top-center
- Top-right
- Middle-left
- Middle-center
- Middle-right
- Bottom-left
- Bottom-center
- Bottom-right
Common properties exist for all graphic elements.
Property | Category | Purpose | Accepted Values |
Access | Security | Specifies if all users have access to the control element, or if access is inherited from the screen. |
|
Angle | Position and Size | Specifies the rotation angle. Enter 180 to display the graphic element upside down. If you enter a value larger than 360, the portion of numeric value that is over 360 becomes the value. For example, enter 380 to see a value of 20. If you enter a value less than 0, the negative value is subtracted from 360. For example, enter -30 to see a value of 330. |
|
Enabled | Appearance | Specifies if the graphic element is available on the HMI device and if the graphic element accepts touch and key input. |
|
Height | Position and Size | Specifies the height in pixels. | Any positive numeric value |
Opacity | Appearance | Specifies the transparency of the graphic element. | 0 (fully transparent) - 100 (fully opaque) |
Visible | Appearance | Specifies if the graphic element is visible on the HMI device. |
|
Width | Position and Size | Specifies the width in pixels. | Any positive number |
X | Position and Size | Specifies the horizontal coordinate, in pixels, from the upper left corner of screen to the upper left corner of a graphic element or group with no rotation. If the graphic element or group is rotated, the X property value does not change. | Any positive number |
Y | Position and Size | Specifies the vertical coordinate, in pixels, from the upper left corner of screen to the upper left corner of a graphic element or group with no rotation. If the graphic element or group is rotated, the Y property value does not change. | Any positive number |
Provide Feedback