Automatic Diagnostics History Medium
The Automatic Diagnostics History table for a seven-inch HMI device is predefined to display history of automatic diagnostics state changes.
Use the Automatic Diagnostics History table to:
- View history of state changes for automatic diagnostics
- View history of state changes details of an automatic diagnostic.
Built-in animation properties
Name | Category | Purpose | Accepted values |
|---|---|---|---|
DateTimeFormat | General | Specifies the format of the date and time displayed for an automatic diagnostics | Any selection option |
Unique properties
Unique properties are properties that not all graphic elements in the
Toolbox
share.Name | Category | Purpose | Accepted values |
FontName | Appearance | Specifies the font of the text. | Any selected font |
FontSize | Appearance | Specifies the size of the text. | Positive numbers |
RowPadding | Appearance | Specifies the distance, in pixels, between the cell contents and the cell border. | Any positive number |
SortOrder | Appearance | Specifies the columns to sort as well as the sort order. | A valid column number, colon, and a D for descending or A for ascending. |
FilterIndex | Appearance | Specifies the default filter for an automatic diagnostics table. The number of the filter represents the order in which the filter appears on the Filters tab. Entering 3 in the FilterIndex property initially filters the automatic diagnostics on the HMI device by third filter that appears on the Filters tab. | Any positive number |
HelpEnabled | Appearance | Specifies if the help button is available on the HMI device. |
|
SuppressEnabled | Appearance | Makes the Suppress button available.When enabled, the button is available and accepts touch or key input on the HMI device. When not enabled, the button is not available and does not accept touch or key input. The button has a crosshatch overlay on top of it to indicate it is not available. |
|
UnsuppressEnabled | Appearance | Makes the Unsuppress button available.When enabled, the button is available and accepts touch or key input on the HMI device. When not enabled, the button is not available and does not accept touch or key input. The button has a crosshatch overlay on top of it to indicate it is not available. |
|
SuppressAccess | Security | Specifies if all users have access to the Suppress button or if access is inherited from the screen. |
|
UnsuppressAccess | Security | Specifies if all users have access to the Unsuppress button or if access is inherited from the screen. |
|
Common properties
Common properties exist for all graphic elements.
Property | Category | Purpose | Accepted Values |
Access | Security | Specifies if all users have access to the control element, or if access is inherited from the screen. |
|
Angle | Position and Size | Specifies the rotation angle. Enter 180 to display the graphic element upside down. If you enter a value larger than 360, the portion of numeric value that is over 360 becomes the value. For example, enter 380 to see a value of 20. If you enter a value less than 0, the negative value is subtracted from 360. For example, enter -30 to see a value of 330. |
|
Enabled | Appearance | Specifies if the graphic element is available on the HMI device and if the graphic element accepts touch and key input. |
|
Height | Position and Size | Specifies the height in pixels. | Any positive numeric value |
Opacity | Appearance | Specifies the transparency of the graphic element. | 0 (fully transparent) - 100 (fully opaque) |
Visible | Appearance | Specifies if the graphic element is visible on the HMI device. |
|
Width | Position and Size | Specifies the width in pixels. | Any positive number |
X | Position and Size | Specifies the horizontal coordinate, in pixels, from the upper left corner of screen to the upper left corner of a graphic element or group with no rotation. If the graphic element or group is rotated, the X property value does not change. | Any positive number |
Y | Position and Size | Specifies the vertical coordinate, in pixels, from the upper left corner of screen to the upper left corner of a graphic element or group with no rotation. If the graphic element or group is rotated, the Y property value does not change. | Any positive number |
Provide Feedback