Alarm History Large
The Alarm History table for a nine-inch HMI device is predefined to display the history of alarm state changes.
Use the Alarm History table to:
- View history of state changes for alarms
- Filter alarm state changes
- View history of state changes for individual conditions of an alarm.
Built-in animation properties
Name | Category | Purpose | Accepted values |
|---|---|---|---|
DateTimeFormat | General | Specifies the format of the date and time displayed for an alarm | Any selection option |
SelectedAlarmName | General | The name of the selected alarm in the alarm table on the HMI device. | Any alarm name in a controller. Tip: This property is not bindable. |
Unique properties
Name | Category | Purpose | Accepted values |
|---|---|---|---|
FontName | Appearance | Specifies the font of the text | Any selection font |
FontSize | Appearance | Specifies the size of the text. | Positive numbers |
RowPadding | Appearance | Specifies the distance, in pixels, between the cell contents and the cell border. | Any positive number |
Enabled | Appearance | Disable touch and key input for an alarm table to prevent interaction with the table on the HMI device. For example, disable touch and key input for an alarm table to prevent selecting alarms on the HMI device. |
|
RefreshEnabled | Appearance | Makes the Refresh button available. When enabled, the button is available and accepts touch or key input on the HMI device. When not enabled, the button is not available and does not accept touch or key input. The button has a crosshatch overlay on top of it to indicate it is not available. |
|
HelpEnabled | Appearance | Specifies if the help button is available on the Alarm History. |
|
SortOrder | Appearance | Specifies the columns to sort as well as the sort order. | A valid column number, colon, and a D for descending or A for ascending. For example, 1:D,2:D provides a primary sort of Column 1 in descending order, and a secondary sort of Column 2 in descending order. You can enter a value for each column in the table. Tip: This property is not bindable. |
Common Properties
Name | Category | Purpose | Accepted values |
|---|---|---|---|
Opacity | Appearance | Specifies the transparency of the graphic element. | 0 (fully transparent) - 100 (fully opaque) |
Visible | Appearance | Specifies if the graphic element is visible on the HMI device. |
|
Enabled | Appearance | Specifies if the graphic element is available on the HMI device and if the graphic element accepts touch and key input. |
|
X | Position and Size | Specifies the horizontal coordinate, in pixels, from the upper left corner of screen to the upper left corner of a graphic element or group with no rotation. If the graphic element or group is rotated, the X property value does not change. | Any positive number |
Y | Position and Size | Specifies the vertical coordinate, in pixels, from the upper left corner of screen to the upper left corner of a graphic element or group with no rotation. If the graphic element or group is rotated, the Y property value does not change. | Any positive number |
Width | Position and Size | Specifies the width in pixels | Any positive number |
Height | Position and Size | Specifies the height in pixels | Any positive numeric value |
Angle | Position and Size | Specifies the rotation angle. Enter 180 to display the graphic element upside down. If you enter a value larger than 360, the portion of numeric value that is over 360 becomes the value. For example, enter 380 to see a value of 20. If you enter a value less than 0, the negative value is subtracted from 360. For example, enter -30 to see a value of 330. | Numbers 0 to 360 |
Provide Feedback