Time lead and follow up
Set a controller with Smart Objects as a time lead or time follower.
A controller can be either a time lead, time follower or neither. If a controller is a time leader the system sets
raC_SO_SOG.A.2
to True
and raC_SO_SOG.A.3
to False
. If a controller is a time follower, the system sets raC_SO_SOG.A.2
to False
and raC_SO_SOG.A.3
to True
. If a controller is neither the system setsraC_SO_SOG.A.2
to False
and raC_SO_SOG.A.3
to False
. On connection to a controller the system reads the values and determines the time configuration.Provide Feedback