Install base code
Open the desired Logix application in
Studio 5000 Logix Designer
and then launch Studio 5000 Smart Object Configurator
.Connect to a
Studio 5000 Logix Designer
.acd
project file to run Studio 5000 Smart Object Configurator
. To create a FactoryTalk Smart Object
, the .acd
project file requires FactoryTalk Smart Object
base code: program, routine, and rung. If
FactoryTalk Smart Object
base code is not in the project, install the FactoryTalk Smart Object
base code. To install base code
- Double-click an.acdproject file.
- InStudio 5000 Logix Designer, selectTools >.Studio 5000 Smart Object ConfiguratorIf the project includesFactoryTalk Smart Objectbase code,Studio 5000 Smart Object Configuratorlaunches with theFactoryTalk Smart Objectinformation model.
- IfFactoryTalk Smart Objectbase code is not in the project, install theFactoryTalk Smart Objectbase code.
- InInsert base componentsselect a program. The program can be in the fastest executing task within the project.
- Select a routine. The routine must be ladder logic.
- Select a rung number.
- SelectAdd.Code is injected into the controller. TheAssetstab in theController Organizerupdates. AFactoryTalk Smart Objecttimer appears in the ladder logic according to the location set for theFactoryTalk Smart Objectbase code. A first element calledInformation modelappears inStudio 5000 Smart Object Configurator.
Provide Feedback