Refresh a model

To import changes you make in
Studio 5000 Logix Designer
into
Studio 5000 Smart Object Configurator
, refresh the information model. Refreshing the model ensures that model information match in both
Studio 5000 Logix Designer
and
Studio 5000 Smart Object Configurator
.
TIP:
If the safety controller lock is enabled, the SOC fails to update the controller. The workaround is to unlock it to refresh the model.
If the safety controller is signed, remove the signature before editing Smart Objects (resigning a controller can invalidate any safety network associated with that signature).
To refresh a model
  1. Make changes in
    Studio 5000 Logix Designer
    .
  2. In
    Studio 5000 Smart Object Configurator
    , select
    Refresh information model
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal