Configure UDTs
Configure UDTs in Studio 5000 Logix Designer before adding them to Smart Object Configurator.
User can browse all UDTs located in ACD file and review UDT SO names, member names, member types, structure, when creating an Smart Object.
Data types available in UDT are Boolean, short integers, integers, double integers, long integers, reals, long reals (for V34 and higher), string, custom length strings, and arrays.
Member data types available in UDT are SINT, INT, DINT, LINT, Boolean, Real, LReal, and String (also custom length strings). Arrays with all these data types are also available.
Provide Feedback