Edit an AOI with existing FactoryTalk Smart Object instances
When created, an Add-On Instruction inherits values from the definition. You must manually push new Add-On Instruction definition changes to the instances of the Add-On Instruction with FactoryTalk Smart Object instances.
To edit an Add-On Instruction with existing FactoryTalk Smart Object instances
- SelectConfigure AOIs.
- Select an Add-On Instruction.
- Verify that the Add-On Instruction model is correct.
- In Studio 5000 Logix Designer, go to the logic of the Add-On Instruction and then monitor a tag.
- InCopy default values to tags of type, selectCopy Specified Values.
- Select the local tag for the modifiedFactoryTalk Smart Objectand then selectOK.
- Download the Studio 5000 Logix Designer project to a controller or emulator.
- Put the controller in Run mode for at least 5 seconds. Save and then upload the values.
- InStudio 5000 Smart Object Configurator, selectRefresh information model.The information models reflect the changes.TIP:To delete aFactoryTalk Smart Objectinside an Add-On Instruction, inStudio 5000 Logix Designerdelete the code and backing tag. ReconnectStudio 5000 Smart Object Configurator. There is no need to download the project.
Provide Feedback