Failed to remove force
This message is displayed when you try to remove a force from a transition or forced (false) simultaneous branch leg. This error can only happen in extreme conditions, such as the controller is switched to hard run mode just after you attempt to remove the force.
Provide Feedback