View Safety Status and Signature

When there is a Safety controller, the controller safety status, safety lock state, and safety signature information can be viewed using the
Safety Status
button on the Online Bar and the
Safety
tab on the
Controller Properties
dialog.
The Safety signature consists of an ID, Date, and Time. The date and time values correspond to when the signature was generated. The ID is a unique value calculated by the controller over the memory contents at the time the signature is generated.
TIP:
Compact GuardLogix
5380 and
GuardLogix
5580 controllers have a 32 byte ID. Only the first 4 bytes of the ID display on the screen. Select Browse button to view and copy the entire 32 byte ID.
To view safety status and signature information:
  • The
    Safety Status
    button on the Online Bar shows the safety status states, whether the controller is safety-locked or -unlocked, or faulted.
    • Select the
      Safety Status
      button to view the Safety signature when a Safety signature exists.
    • Select the
      Controller Properties
      icon and then select the
      Safety
      tab to view the safety status and signature information on the
      Controller Properties
      dialog.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal