Current Reference page
Use the settings on the
Current Reference
page in the Axis Properties
dialog box to configure the low pass filter bandwidth and the notch filter frequency for a converter. The
Current Reference
page is available when, on the General
page, the Axis Configuration
is set to Regenerative AC/DC Converter
or Low Harmonic AC/DC Converter
.The parameters are unavailable when in online mode and when the axis is
Servo On
.
TIP:
To open the Current Reference page:
- In theController Organizer, expand theMotion Groupsfolder, and double-click an axis.
- From theAxis Propertiesdialog box, inCategories, selectGeneral.
- In theAxis Configurationbox, selectRegenerative AC/DC ConverterorLow Harmonic AC/DC Converter.
- InCategories, selectCurrent Reference.
Parameter | Description |
|---|---|
Low Pass Filter Bandwidth | Specifies the break frequency for the low pass filter applied to the active current reference signal. The default is 0.0 Hertz. |
Notch Filter Frequency | Specifies the center frequency of the notch filter applied to the active current reference signal. The default is 0.0 Hertz. |
Parameters | Opens the Master Axis Parameters page to configure additional current reference parameters. |
Provide Feedback