Autotune page
Use the
Autotune
page to perform an autotune to improve the performance of the system.
TIP:
Autotune
category is available only when Axis Configuration
on the General
page is set to Position Loop
or Velocity Loop
.
TIP:
To open the Autotune page:
- In theController Organizer, expand theMotion Groupsfolder, and double-click an axis.
- From theAxis Propertiesdialog box, inCategories, clickAutotune.
This table describes the settings on the page:
Parameter | Description |
Application Type | Used to select the type of application to be tuned. The available values include:
The default value is Basic .
TIP:
Changing the Application Type value affects
other attributes (Velocity Integrator Hold, Position Integrator Hold, Gain Tuning
Configuration Bits).
Application Type is unavailable when the axis is Servo On. |
Loop Response | Used to select how tightly or hot the system tunes. The available values include:
The default value is the current value of the attribute.
TIP:
Changing the Loop Response value affects the
Damping Factor attribute.
Loop Response is unavailable in online mode and when the axis is Servo On. |
Load Coupling | Used to select how tightly the system is physically coupled. The available values include:
The default value is the current value of the attribute. Applying changes to the Coupling value causes changes to the gain values that are displayed in the Gains Tuned grid in the right panel of the Autotune tab.Load Coupling is unavailable in online mode and when the axis is Servo On. |
Position Integrator Bandwidth | Used to calculate the position integrator bandwidth. The position integrator bandwidth only applies when the Axis Configuration on the General tab is set to Position Loop . When the Axis Configuration is not set to Position Loop , this control is unavailable and you cannot modify it.When Application Type is set to Custom and the application is in offline mode, this check box is enabled and you can modify the setting.Position Integrator Bandwidth is unavailable:
|
Velocity Integrator Bandwidth | Used to calculate the Velocity Integrator Bandwidth .When Application Type is set to Custom , this check box is enabled, and you can modify the setting. Velocity Integrator Bandwidth is unavailable:
|
Velocity Feedforward | Used to calculate the Velocity Feedforward .The Velocity Feedforward only applies when the Axis Configuration on the General tab is set to Position Loop . When the Axis Configuration is not set to Position Loop , this control is unavailable and you cannot modify it.When Application Type is set to Custom , this check box is enabled. and you can modify it. Velocity Feedback is unavailable:
|
Acceleration Feedforward | Used to calculate the Acceleration Feedforward .When Application Type is set to Custom , this check box is enabled. and you can modify the setting.Acceleration Feedback is unavailable:
|
Torque Low Pass Filter | Used to calculate the Torque Low Pass Filter .When Application Type is set to Custom , this check box is enabled, and you can modify the setting. Torque Low Pass Filter is unavailable:
|
Measure Inertia using Tune Profile | Used to calculate the Inertia Tuned values as part of the Autotune. The Inertia Test results are shown in the Inertia Tuned grid control (bottom right of this tab) when the test completes. Measure Inertia is unavailable in offline mode as well as in online mode when the axis is Servo On. |
Motion with Load | Used to calculate information based on the load inertia. The load inertia is measured and applied to the Total Inertia attribute or Total Mass attribute. If the value for Rotary Motor Inertia or Linear Motor Mass is non-zero, the Load Ratio is also updated. Total Inertia and Rotary Motor Inertia apply to rotary motors. Total Mass and Linear Motor Mass apply to linear motors.The blue arrow next to a control indicates that the data is immediately committed. You cannot undo the selection. Motion with Load is unavailable:
|
Uncoupled Motor | Used to calculate information based on the motor inertia. If selected, when the test is run, the motor inertia is measured and is stored in the Rotary Motor Inertia attribute or Linear Motor Mass attribute. Rotary Motor Inertia applies to rotary motors. Linear Motor Mass applies to linear motors.The blue arrow next to a control indicates that the data is immediately committed. You cannot undo the selection. Uncoupled Motor is unavailable:
|
Travel Limit | Used to specify the maximum distance to travel for the tune operation. The blue arrow next to a control indicates that the data is immediately committed. You cannot undo the selection. Travel Limit is unavailable:
|
Speed | Used to specify the speed of the tune operation. The blue arrow next to a control indicates that the data is immediately committed. You cannot undo the selection. Speed is unavailable:
|
Torque | Used to enter a value that specifies the torque value that is to be applied to the tune operation. The default value is 100. The blue arrow next to a control indicates that the data is immediately committed. You cannot undo the selection. Torque is unavailable:
|
Direction | Used select the direction of the move for the tune operation. The available values include:
The default value is Forward Unidirectional .The blue arrow next to a control indicates that the data is immediately committed. You do not have the opportunity to undo the selection. Direction is unavailable:
|
Start | Used to initiate an autotune operation. When the Measure Inertia check box is selected, a request is issued to the controller to start a tune. Pending edits need to be applied before you start the test. If you have pending edits, a dialog box opens informing you that pending edits will be applied prior to executing the test. You can choose Yes or No to apply the pending edits. If you choose No, the test will not be executed. Clicking the Start button issues a Motion Direct Command to the controller, which causes any parameters used by the Motion Direct Command to validate before starting the test. If the Motion Direct Command does not execute due to an error condition, an error message displays and the Test State returns to the Ready state Start is unavailable:
|
Stop | Used to terminate an autotune operation that was started somewhere other than the Autotune dialog box that is displayed. When an Autotune is started from the Start button on this dialog box, this Stop button is not available.This Stop button is only available if the Autotune was started from the user program Motion Run Axis Tuning (MRAT) or when multiple workstations are used and the Autotune is started from a different workstation.The stop tune issues a Motion Direct Command to the controller. Stop is unavailable:
|
Danger | Used to displays warning information about the tuning operation. Danger text is unavailable in offline mode and when the Measure Inertia check box is not selected. |
Tune Status | Used to display the status of the tuning operation. Tune Status values include:
The default value is Ready. |
Loop Parameters Tuned | Contains one column that lists the current attributes and one column that lists the calculated results of the tuning operation. |
Rows Header | Contains a splat (*) when the Tuned Value is not the same as the Current Value. |
Name | Displays the name of the attribute. |
Current Value | Displays the value of the gain attribute from the controller. |
Tuned Value | Contains the tuned value for the attribute. Tuned Values may be calculated by the autotune. When a gain is no longer used in the tune calculation (the corresponding check box in the Customize Gains to Tune group is not selected), the Tuned Value is set to zero. The tuned value column becomes blank until a tune operation is started. Once started, the data updates, regardless of the completion status. |
Unit | Contains the units that are associated with the corresponding attribute.
TIP:
Attributes that do not apply to the current
configuration are not shown in the grid.
|
Advanced Compensation | Used to expand and the minus sign to collapse the Advanced Compensation section.The default is that the Advanced Compensation section is collapsed.The Advanced Compensation section is unavailable in offline mode as well as in online mode when the axis is Servo On. |
Inertia | Used to enter an inertia value to be used in tuning calculations. If the Use Load Ratio check box is selected on the Load dialog box, this attribute is a measure of load ratio. Otherwise, this attribute is a measure of tune inertia mass.Inertia is unavailable:
|
Compensate check box for Inertia | Used to calculate the inertia value in the tuning procedure. The Compensate check box for Inertia is unavailable:
If you run the tune operation with Measure Inertia selected, the controller returns the inertia value. If Inertia is checked, the value is used in the tune equations. You can enter a different inertia value, then re-run the tune calculations using the specified value. |
Friction | Used to enter a friction value in tuning calculations. Friction is unavailable:
|
Compensate check box for Friction | Used to calculate the Friction value in the tuning procedure. The Compensate check box for Friction is unavailable:
If you run the tune operation with Measure Inertia checked, the controller returns the friction value. You can enter a different friction value, then re-run the tune calculations using the specified value. |
Active Torque | Used to enter an active torque value in tuning calculations. Active Torque is unavailable:
|
Compensate check box for Active Torque | Used to calculate the active torque value in the tuning procedure. The Compensate checkbox for Active Torque is unavailable:
If you run the tune operation with Measure Inertia selected, the controller returns the active torque value. You can enter a different active torque value, then re-run the tune calculations using the specified value. |
Calculate Compensation | Used to calculate the compensation values. Calculate Compensation is unavailable in offline mode. |
Load Parameters Tuned | Contains one column that lists the current attributes and one column that lists the calculated results of the tuning operation. |
Rows Header | Contains an asterisk (*) when the Tuned Value is not the same as the Current Value. |
Name | Used to displays the name of the attribute. |
Current Value | Used to displays the value of the gain attribute from the controller. |
Tuned Value | Contains the tuned value for the attribute. One column lists the current attributes and one column lists the calculated results of the tuning operation. Tuned Values may be calculated by the autotune. When a gain is no longer used in the tune calculation (that is, the corresponding check box in the Customize Gains to Tune group is not selected ), the Tuned Value is set to zero. The tuned value column becomes blank until a tune operation is started. Once started, the data updates, regardless of the completion status. |
Unit | Contains the units that are associated with the corresponding attribute.
TIP:
Attributes that do not apply to the current
configuration are not shown in the grid.
|
Accept Tuned Values | Used to commit the values from the Tuned Value columns of the grid to the attribute, causing the Current Value column to update. The blue arrow next to a control indicates that the data is immediately committed. You do not have the opportunity to undo the change. The Accept Tuned Values button is unavailable in offline mode and if no test was successfully completed. |
Provide Feedback