Failed to convert an older project file

Problems and Solutions
Problem - The project file was not converted because:
Solution - To resolve the problem:
Do not have the required security permission to access the project.
Check with your Security Administrator to verify sufficient access to the project.
One or more components in the project are protected by License Source Protection, and the
CmStick
containing the license is not present on the computer.
Insert the appropriate
CmStick
containing the required license. Refer to the error message to see the firm code and product code of the missing license.
One or more components in the project are protected by License Source Protection, which is not supported on the selected controller in this version of the
Logix Designer
application.
Remove License Source Protection from the project or components before importing them, or open the project using a
ControlLogix
5570 controller or a
CompactLogix
5370 controller.
One or more safety components in the project are protected by License Source Protection. which is not supported on the selected controller in this version of the
Logix Designer
application.
Compact GuardLogix 5380, CompactLogix 5380, ControlLogix 5580, and GuardLogix 5580 controllers
do not support License Source Protection for safety components.
Open the recovery file in the version of the
Logix Designer
application in which it was created. That application version presents the option to use the recovery file or the last saved file version.
The
Logix Designer
application found a recovery file for the project to open. The recovery file was created in an older version of
Logix Designer
than is currently installed.
Delete the recovery file from the system and try converting it again.
Tip:
If the recovery file is hidden, it does not appear in your directory. Show hidden files to view all files.
The project contains a safety signature that is incompatible with the new controller version.
Generate a new safety signature for the project. See Controller Properties dialog box - Safety tab settings for more information on safety signatures.
Contact
Rockwell Automation
Technical Support for assistance if you continue to have difficulty converting the file.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal