Vendor Sample Projects command
Choose this command to launch the
Vendor Sample Projects .pdf
file to access sample projects from Rockwell Automation and several other vendors. Use these sample projects with products from those companies. Refer to the PDF file for more information.
IMPORTANT:
Some browsers (particularly the Edge browser)
will not launch the
Logix Designer
application from the ACD
hyperlinks in the PDF file when configured to open PDF files.Provide Feedback