Find a function within a DLL file
An external routine DLL must call a function. Use the
Functions Available
dialog to choose a function from a list.To find a function within a DLL file
- From the Controller Organizer right-click the active routine and then chooseProperties.
- Click theConfigurationtab, and then click theBrowse
button. - From the list of available functions, choose the function that the external routine calls.
- SelectOKto close theFunctions Availabledialog.
Provide Feedback