Sequence Execution & Monitoring
Sequence execution is responsible for coordinating:
- The execution of phases in the order specified by the sequence diagram.
- The transition expressions to specify when steps are attached to phases, started, stopped, reset, and attached.
- The step activation to trigger passingEquipment Sequenceinput data to theEquipment Phase.
- The COMPLETE, STOPPED, or ABORTED triggers passing output data from theEquipment Phaseto theEquipment Sequence.
- Generating events to record changes in status and operator interactions.
Equipment Sequence
programs are IDLE until they are started. Resetting an Equipment Sequence
returns them to an IDLE state. Sequence parameters and step tags can be initialized manually or configured as a sequence property.Monitoring is performed from the
Logix Designer
application and the SequenceManager
Controls. The Equipment Sequence
Monitor is the equivalent of the Sequence Detail Control and the Sequence Parameter Control. The rendering of status is the same. Command interactions are the same with the exception of ownership; the Logix Designer
application overrides ownership of the Equipment Sequence
and the SequenceManager
Controls request ownership. Provide Feedback