Failed to set modify trend properties - Samples should be in the range of <Low Limit> - <High Limit>

The
Samples
value is invalid. Enter a valid
Samples
value that is a range from a low of 0 samples to a high of 1000 samples.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal