Configuring Communications for the MSG Instruction
Use the MSG instruction to:
- program a block transfer between the controller and a Remote I/O (RIO) block transfer module. A named RIO module entry (RIO-MODULE) must exist in the Controller Organizer I/O Configuration module tree in order for block transfers to occur.
- send a broadcast message to a receiving controller using the controller's serial port.
- enable large connection support for messages (if the target module supports large packets).
TIP:
Logix Designer versions 37 and later do not support
controllers with serial ports. The
Broadcast
button appears only in Logix Designer
versions 36 and earlier for controllers with a serial port.To configure communications:
- Do one of the following:
- Select thePathbutton to specify a path.In the Path field, type the path or click theBrowsebutton to find the desired module in the module tree.TIP: The module must have a name to be the target of block transfers.
- Select theBroadcastbutton to send a broadcast message, and then select the channel used to send the message.The message path is set to 2,255 for channel 0 or 3,255 for channel 1.TIP: This option is enabled only when you choose a compatible system protocol and a write message type.
- Select the Communication Method for the message. Choose whether the message is routed via CIP,DH+link, or CIP with Source ID.TIP: Broadcast messages only support the CIP communication method.
- Check/clear the Connected box to indicate whether the message is to be sent Connected or Unconnected. This field is enabled only for CIP Generic messages except when theBroadcastbutton is selected. Broadcast messages only support unconnected messages.TIP: If the target device does not support connected CIP messages and this box is checked, an error appears when the message instruction is executed.
- Check or clear theCache Connectionsoption.
- If this option is checked, the controller keeps the connection open after it completes the block transfer.The next block transfer uses the open connection and avoids the delay required to open the connection.
- If this option is cleared, the controller closes the connection after the block transfer operation is complete.Selecting the option results in faster block transfers, but indefinitely retains a connection. Since the controller has a limited number of connections, this could eventually result in the controller being unable to establish connections.
- Select theLarge Connectionsbox to allow the CIP Generic type messages to use a large connection size (4002 bytes) for message transmissions. This check box is enabled only when theConnectedbox is selected, and CIP Generic is selected as the message type on theConfigurationtab.TIP: Not all service types under the CIP Generic message type support Large Connections. Before selecting a large connection, make sure the device (determined by the communication path), service, class, instance and attribute support this feature. If you select an invalid service type, an error message displays.
- SelectOK.
Accessing the Message Configuration dialog box, Communications tab
To access the Message Configuration dialog box, click the Tag Editor to make it the active window, and then click the
button to the right of the MESSAGE operand. From the
button to the right of the MESSAGE operand. From the Message Configuration
dialog box, select the Communications
tab.Provide Feedback