Select a Drive NV as the data source
The Drive NV data source derives motor attributes from the nonvolatile memory of a drive.
To select Drive NV as the data source:
- From theAxis Propertiesdialog box, inCategories, clickMotor.
- In theMotor Device Specificationarea, in theData Sourcelist, clickDrive NV.
- In theUnitslist, select the motor units that are associated with the motor.TIP:For a rotary motor, selectRev. For a linear motor, selectMeter.
- SelectApply.
Provide Feedback