Coordinate System Properties - Joints
Use the settings on the
Joints
tab in the Coordinate System Properties
dialog box to define the Joints Conversion ratios. Joint axis units are specified in degrees. The
Joints
tab is available only if you are configuring non-Cartesian coordinate systems.
TIP:
To open the Joints tab:
- In theController Organizer, expand theMotion Groupfolder, and double-click the coordinate system.
- On theCoordinate System Propertiesdialog box, click theJointstab.
Provide Feedback